This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

fatal error #1965: cannot open source file - but file is in project

Other Parts Discussed in Thread: CONTROLSUITE

Hello all!

I am developing for an F28335 in C++ and CCS v5.5 under Windows 7 at the moment.I make a heavy use of subdirectories for my code files and include them via include "relative paths"

During my builds I get sometimes errors that confuse me a bit:


================================================================

"C:\\ti\\ccsv5\\utils\\bin\\gmake" -j 8 TaskScheduler/MeasDataSynchronizer/MeasDataSynchronizer.obj
'Building file: ../TaskScheduler/MeasDataSynchronizer/MeasDataSynchronizer.cpp'
'Invoking: C2000 Compiler'
"C:/ti/ccsv5/tools/compiler/c2000_6.2.0/bin/cl2000" -v28 -ml -mt --float_support=fpu32 --fp_reassoc=off --include_path="C:/ti/ccsv5/tools/compiler/c2000_6.2.0/include" --include_path="<<my project path>>/ACDC_Controller/ObserverPattern/" --include_path="C:/ti/xdais_7_21_01_07/packages/ti/xdais" --include_path="C:/ti/controlSUITE/device_support/f2833x/v133/DSP2833x_headers/include" --include_path="C:/ti/controlSUITE/device_support/f2833x/v133/DSP2833x_common/include" --include_path="C:/ti/controlSUITE/libs/math/IQmath/v15c/include" --include_path="C:/ti/controlSUITE/libs/math/FPUfastRTS/V100/include" -g --define="_DEBUG" --define="LARGE_MODEL" --quiet --verbose_diagnostics --diag_warning=225 --display_error_number --issue_remarks --output_all_syms --cdebug_asm_data --preproc_with_compile --preproc_dependency="TaskScheduler/MeasDataSynchronizer/MeasDataSynchronizer.pp" --obj_directory="TaskScheduler/MeasDataSynchronizer"  "../TaskScheduler/MeasDataSynchronizer/MeasDataSynchronizer.cpp"
"..\TaskScheduler\MeasDataSynchronizer\..\..\ADCController\..\ObserverPattern\AdcMeas\..\..\ADCController\..\GlobalSettings\Controller/ControllerOperationalSettings.h", line 13: fatal error #1965:
          cannot open source file
          "ControllerOperationalSettingsObserverServer.h"
  #include "ControllerOperationalSettingsObserverServer.h"
                                                          ^

1 catastrophic error detected in the compilation of "../TaskScheduler/MeasDataSynchronizer/MeasDataSynchronizer.cpp".

===================================================================.

The error happens in a file that is in the same subdirectory as the included one (hence I use #include "ControllerOperationalSettingsObserverServer.h"). Both files are part of the eclipse project and not included via an include path option.

I had this problem a bit earlier already with another often used file. When I added this project folder to the project includes (--include_path) the error went away.

However, since this is a project file and not a library I do not want to include everything to the includes.

The folder structure is the following way:

  • eclipse project dir
    • TaskScheduler
      • MeasDataSynchronizer
        • MeasDataSynchronizer.h
    • GlobalSettings
      • Controller
        • Controller ... .h

When I look at the compiler output, the last line is confusing to me: why does the path begin with a "../"? What's the base directory to that?
Other than that, I'm just confused why this error pops up and I would like to solve it without playing with --include_path (since all these files are in my eclipse project).

Thanks a lot!

  • Hello,


    So to be clear, is the below accurate?

    • eclipse project dir
      • TaskScheduler
        • MeasDataSynchronizer
          • MeasDataSynchronizer.cpp
      • GlobalSettings
        • Controller
          • ControllerOperationalSettings.h
          • ControllerOperationalSettingsObserverServer.h

    And ControllerOperationalSettings.h has a statement:

    #include "ControllerOperationalSettingsObserverServer.h

    ?

    ab cd said:
    why does the path begin with a "../"? What's the base directory to that?

    The base directory is the current windows directory. That would normally be the active build configuration subfolder (ex. Debug)

    ki

     

  • Ki-Soo Lee said:

    So to be clear, is the below accurate?

    • eclipse project dir
      • TaskScheduler
        • MeasDataSynchronizer
          • MeasDataSynchronizer.cpp
      • GlobalSettings
        • Controller
          • ControllerOperationalSettings.h
          • ControllerOperationalSettingsObserverServer.h

    Yes, that is accurate.

    Ki-Soo Lee said:

    And ControllerOperationalSettings.h has a statement:

    #include "ControllerOperationalSettingsObserverServer.h

    ?

    Yes it does.

    Thanks for the explanation. That makes a lot of sense.

  • Could you provide the .project, .cproject and .ccsproject files in your project folder? I'd like to take a peek at the contents of it.

    Thanks

    ki