This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Importing with copy causes project to be saved in workspace sub-directory

Guru 20035 points

Hello,

When I Import (with copy) a  project into a workspace, it stores the project and associated files in a sub-directory having the same name as the project.

I would like it to just copy the project over to the workspace root directory.

Is that possible?  If not, is there another way to make it happen that way?

Stephen 

  • hi Stephen,

    stevenh said:
    I would like it to just copy the project over to the workspace root directory.

    You cannot specify the workspace folder to be the project folder (the folder containing the .*project files is also known as the project folder). Eclipse will not support this.

    ki