This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cannot view Disassembly in CCS V5.5

I am running  CCS Version: 5.5.0.00077.

This has been working adequately for some time, but suddenly it has decided to stop displaying any disassembly information. I note that a similar problem was discussed a while ago and the solution was to advance to V5.2!

How do I get the disassembly window working, as without it, CCS is useless to me. I am not running a project; I use CCS to investigate the state of a running program that was not created with CCS.

Up to now, opening CCS, selecting a target configuration, and connecting a core has resulted in the disassembly window opening automatically. Now it simply says 'No source available for "0x1080002c"' and the View Disassembly button does nothing.

  • Hello,

    To open the disassembly window, try manually opening it via 'View -> Disassembly'

    Peter Robertson said:
    Up to now, opening CCS, selecting a target configuration, and connecting a core has resulted in the disassembly window opening automatically. Now it simply says 'No source available for "0x1080002c"' and the View Disassembly button does nothing.

    The I'm not sure if the disaassembly view is supposed to auto-open on connect but it should definitely open when you press the button. Try resetting the perspective and see if that helps things.

    Thanks

    ki