This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have big troubles with the latest CCS (Version: 6.0.0.00190) : when I create a new workspace I can compile and debug my projects , but after closing and reopening my workspace it is no more possible to compile and debug, and in the console I have :
Cannot run program "make" : Launching failed
Error: Program "make" not found in PATH
I tried several times to reinstall (uninstall, delete directory...), no improvment. I tried on 2 different computers (Windows Seven 32bits and 64 bits) with the same result again.
The only mean to work (because I need to produce ...) is to delete the .metatdata directory, then opening my workspace (thus create a new one) and then import all my projects in this workspace. I have to repeat this operation each time I open a workspace, It is really tricky.
So, please, I need some suggestions to workaround this problem.
I also notice that to create .txt file I obtain a .hex file, but it seems to be already a known issue.
Thanks
Peter
Hi Peter,
Would you be able to re-create this failure with one, preferably simple, project, and then zip your entire workspace and upload it here?
Thanks,
- Baltasar
Hi,
to answer to your request I have created new workspace and new project on my desktop, but I was unable to recreate the failure. Actually it seems it depends on the directory naming. I did the same in my work directory and then I reproduce the problem.
All my workspaces are on a USB drive and a typical directory is like that (I only change the company name) :
V:\1--- CompanyName ---\MSP430-dev\100 workspaceTest
I used the same directory naming with previous version (CCS v5, v4, v3 ...) without any problem.
Can you try with this naming ?
Regards
Peter
Hi Peter,
I cannot reproduce the problem using the same workspace path on CCS v6.0.0.00190. The issue may have something to do with the fact that your workspace is on a removable drive. Make sure that your workspace directory is fully writeable, and also make sure that the same drive letter (e.g. "V:") is used consistently for all CCS sessions with that workspace.
If you can reproduce the problem on a local drive, please let me know the steps.
Thanks,
- Baltasar
Hi,
It works now.
It is not a problem of local or removable drive. The problem is the "-" (key 6 on my azerty keyboard). When I remove all these "-" in my directories names, it is ok. I have also deleted the space character, preventively...
I have replaced my "-" with "_" (key 8) and it's still ok.
Regards,
Peter