This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem:" Target Endianness doesn't match, Check the Build options or Setup Utility"



Hello ,

I have ccs 2.0 and Emulator drivers from Seed.
I have connected the Emulator (XDS510 USB2.0) to my own hardware
board(cantains single C6713b processor) and I have configured the
ccs in emulator mode. But When I load programs, I am encountering the following problems
-" Target Endianness doesn't match, Check the Build options or Setup Utility". And I
have checked the configuration of the build options and the Setup Utility, They are
all in little endianness.

I don't know what to do at this point.

  • CCS 2.0 is fairly old these days so you may find support somewhat limited, if possible you may want to try out a newer version of CCS. As to the issue, are you certain your C6713 is properly configured to little endian so it matches the build options? Just as a test it may be worth trying to set your build options to big endian to see if it will allow you to load, this should prove if it is really an endianess issue or something else going wrong behind the scenes. You may also want to check with Seed to ensure you have the latest driver package for your particular version of CCS.

  • Thanks for your reply.

    The Problem has been solved.There is a hardware mistake. I can connect the board correctly now.