I have several EVMs and a couple of EZDSPs for the C5505. I only want to develop code for the C5505. I don't understand what CCS licenses pertain to me.
We have been using v3.3 and we are restructuring a lot of code right now and so if we should switch to CCS v4.0, then now is the time to do it.
1. Is there a big advantage to using CCS v4 over v3.3? CCS v3.3 seems to be getting the job done okay.
2. Am I already licensed to use v4.0 based on my purchases of the EVMs this past 9 months? Or do I have to pay something more in order to develop and produce code for production?
3. Can some of our developers use v3.3 and others use v4.0 in the same folder? Or will the source code differ between the CCS versions or the studios step on one another when used simultaneously on the same code?
Thanks,
David