Other Parts Discussed in Thread: TMS320F2812
Hi,
IDE : CCS v4.0 (32K MCU Core) Target : TMS320F2812 Emulator : SD SPI 515 Parallel Port JTAG Emulator
I have migrated CCS v3.3 project to CCS v4.0 and build the target successfully with the guidelines from ti web. Now I want to Debug the target. I'm using SD SPI 515 Parallel Port Emulator. I have some problems
1. While creating Target Configuration there's no a Spectrum Digital SPI Parallel Port Emulator listed in the pull down menu. I got a reply from Spectrum Digital Support Team to select XDS 510 PP - PCI Parallel Port Emulator while configuring the target and I followed it.
2. When I tried to start a Debug Session for above Target Configuration I received the following message window indicating You are not licensed to use the currently cofigured target as below
3. Also I notice Unlicensed at the top of the window header
Why it says unlicensed even it is 32K license free? Does it mean Debugging need license?
I found a similar screen shot to activate a free license for XDS100 USB at
http://wiki.davincidsp.com/index.php/XDS100#Q:_Can_I_use_Code_Composer_Studio_v4_with_XDS100.3F
I could successfully Test and Reset the Emulator through SDConfigEx that comes along with CCS v4.0 installation.
Please help to solve the Emulator License Problem. Any web link specifying this?
Thanks in advance
-SBS