This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Been pulling my hair out for 2 weeks now. I had CCSV4.1 and an XDS100V2 emulator working with an f2812 target board, then went off to revise some code and do some other stuff. When I next tried to connect, I kept getting "error initializing emulator". CCSV4.1 also crashes immediately after I click on the cancel button of the error message window. Thought it may have been the emulator, so ordered another. New one is the same. The error appears almost immediately when launch debug is selected. I tried uninstall/reinstall of CCSV4.1 and FTDI drivers multiple times to no avail. I then tried a new download of V4.1, no joy! Now I have most recently downloaded and installed V4.1.1, still the same response. If I set the configuration to the TI simulator, debug works fine on my project code. (I went back to the project I originally successfully connected, loaded, and ran - so its not related to my code). I also have loaded the same code onto the target using CCSV2.2 and an XDS510pp emulator to verify the jtag port on the target board was ok. Can't use this for the new project as the ultimate target is an F28235 processor, and it is going to a customer who will need to be able to support on laptops that may not have parallel ports and doesn't want to spend a fortune on purchasing emulators. I spent 2+ years on a project with CCSV2.2 and the XDS510 emulator and can't remember once having these types of problems. What good is a hammer if the head falls off with each strike of the nail?
I hope someone else has seen this problem and has resolved it and can share what was done to fix it!
WhenI get a similar problems, I usually try working it from the lowest level. For me,that means checking the JTAG connection and then working on up to find the problem. I found this wiki helpful: http://www.tiexpressdsp.com/index.php/Debugging_JTAG_Connectivity_Problems (note that the v4 commands are in the middle). Using that article I usually verfiy that the XDS unit is working, the windows drivers are installed OK and the config setup in CCS is correct. If I can get scan path passing, I know it's not the hardware, os drivers, setup or emulation stuff.
The ccs dump files may also be helpful to those supporting CCS: http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/3131.aspx details where to find them.
I have already gone through the connectivity problems wiki process multiple times. There is no dump log generated. The only item in the error log is:
eclipse.buildId=4.1.1.00014
java.version=1.5.0_14
java.vendor=Sun Microsystems Inc.
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=en_US
Command-line arguments: -os win32 -ws win32 -arch x86
Error
Tue Mar 09 00:02:45 EST 2010
Error: C28xx: Error initializing emulator
I have used XDSPROBE and DBGJTAG to check the scan path, all test were succcessful. The target board jtag and processor are working fine, as verified with CCSV2.2 and XDS510PP emulator. Also, the CCSV4.1/XDS100V2 configuration worked 3 weeks ago when V4.1 was first installed - with the same App code and configuration info. My conclusion is there is a problem with CCSV4.1 now that wasn't there during the initial installation - possibly something else interferring with the connection between CCSV4.1 and the emulator drivers. Removing all traces of CCSV4.1 and FTDI drivers and reinstalling from the same distribution that worked originally doesn' change the situation now. I have also tried deleting the workspace and starting from scratch, and also tried a new workspace and the timers example code only, with the same results.
I did find some other log files, don't know if they are of any use or not, but I have attached a zip of them, in case anyone is interested in reviewing them.
No log there. I did a search on .log, and the ones I included previously are all that were found in the CCSV folders. If I unplug the emulator, then run debug, the same symptom occurs - error initializing emulator pops up and when I click on cancel CCSV4.1 disappears and the attached window pops up. (don't know if there is any useful info in it)
Resolved the CCSV crashing problem when opening debug. Uninstalled CCSV, and went through the registry and tried to remove any references to CCSV and XDS100 manually. (I found that FTCLEAN did not actually clean out the USB enum hives - probably due to Win7 restrictions). Then reinstalled CCSV4.1 (last version known to work with the XDS100), and now I can enter debug. Still get the error initializing emulator at start, but canceling the error window doesn't crash CCSV4, it will go into debug mode without the emulator.
HOWEVER, I still cannot communicate with the emulator, and still don't know why. No errors other than the initial 'error initializing emulator', and no idea what to look for, nor what to do next. I have submitted an official problem request to TI AND to Spectrum Digital (sellor of emulator) - NO REPLIES FROM EITHER CO.!!! My once high opinion of both co's is in a rapid downward slide now.
I was using XDS100v2 with 28x today, and encountered a similar problem. However, in my case, the EEPROM was not programmed properly. You may want to check if it is programmed correctly: http://tiexpressdsp.com/index.php/XDS100#Q:_How_can_I_check_if_the_VID.2FPID_for_the_EEPROM_are_programmed_correctly.3F But the error in that case is -150, so it looks a little different.
Can you post the XML from your setup? This is found in the target connections-->source tab. That can show us the relative paths that the CCS is searching for in the dirivers.
Just to recap, were you able to run dbgjtag with the current target configuration set as the default and doing a connectivity test? That would also tell us if the CCS configuration files are generated OK.
DBGJTAG integrity and brokenpath tests both pass each time, using the current board config. When I try "DBGJTAG -A scanpath", I get the following error report:
"The configure file indicates just one JTAG device should be in the system.
This test indicates zero JTAG devices are actually in the system.
This test cannot analyse the scan-path when the
configure file and the scan-path do not match."
I have tried various lines from the config file as the device name, but no different results
The board data file is as below:
# config version=3.5
$ sepk
pod_drvr=jioserdesusb.dll
pod_port=0
pod_serial=SDSMA6OP
$ /
$ product
title="Texas Instruments XDS100v2 USB"
alias=TI_XDS100v2_USB
name=FTDI_FT2232
$ /
$ ftdi_ft2232
usb_vid=0x0403
usb_pid=0xa6d0
gpio_l0="TRSTn,Active_Low"
gpio_l1="EMU_Pin_Enable,Active_Low"
gpio_l2="EMU_Pin_0,Active_Low"
gpio_l3="Adaptive_Clock,Active_High"
gpio_h0="SRSTn,Active_High"
gpio_h1="SRSTn_In,Active_Low"
gpio_h2="Power_Loss_Detect,Active_Low"
gpio_h3="Power_Loss_Reset,Active_High"
gpio_h4="EMU_Pin_1,Active_Low"
gpio_h5="Cable_Disconnect,Active_High"
gpio_h6="Loopback,Active_High"
$ /
$ uscif
tdoedge=FALL
jtagboot_mode=disable
jtagboot_value=hiz
powerboot_mode=disable
powerboot_value=hiz
tclk_program=SPECIFIC
tclk_frequency=1.0
loopback_mode=disable
loopback_value=disable
$ /
@ c28xx family=tms320c28xx
# /
Here is the target configuration XML source, as well. Don't see what relationship this has to anything DBGJTAG is doing.
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="Texas Instruments XDS100v2 USB Emulator_0">
<instance XML_version="1.2" desc="Texas Instruments XDS100v2 USB Emulator_0" href="connections\TIXDS100v2_Connection.xml" id="Texas Instruments XDS100v2 USB Emulator_0" xml="TIXDS100v2_Connection.xml" xmlpath="connections"/>
<connection XML_version="1.2" id="Texas Instruments XDS100v2 USB Emulator_0">
<instance XML_version="1.2" href="drivers\tixds100v2c28x.xml" id="drivers" xml="tixds100v2c28x.xml" xmlpath="drivers"/>
<property Type="choicelist" Value="1" id="Emulator Selection">
<choice Name="Select by serial number" value="0">
<property Type="stringfield" Value="SDSMA6OP" id="-- Enter the serial number"/>
</choice>
</property>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="TMS320F28235_0" href="Devices\f28235.xml" id="TMS320F28235_0" xml="f28235.xml" xmlpath="Devices"/>
</platform>
</connection>
</configuration>
</configurations>
Thanks. We tried to duplicate the error you have and were unable.
We built a special 28x driver to help us debug this problem.
Could you respond to my friend request so we can setup a conference call directly? Thanks.
Ok, thanks. To answer your other question, we were not able to solve WGauss problem. We actually created a special driver to help find the problem, but were not able to get it to WGauss to use it and find the problem.