This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DEBUG SPL with AM3352, Eclipse Juno, JLink Pro, Linaro 4.9.2 toolchain.



Hello,

I have a custom board DDR3, TPS6917 PMIC, SPI boot with NAND flash.

I am trying to debug the SPL by loadinbg the SPL binary, and then loading symbols from the ELF file. All is good, I can start the debugger and I get this window set....

As you can see the SP is pointing at the start vector, and the CPSR has been preloaded to a value with ARM instructions set.

This all looks good but on the first step I get an undefined instruction trap.

I'm confused? This is the exact code that is present in init.S, so its valid startup code.

I can compile the bootloader example with a bare-metal toolchain and run that up. But This little glitch has dumbfounded me.

All i can think is that my register setup is not correct. The CCS instruction for debugging SPL say just clear the T-bit in CPSR and you should be good to go.

Thanks for any info,

Eldon.