This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Multiple data visualization with the single time graph in Code Composer Studio

Hello

I want to visualize some data which will change during time (f.e. logging ADC values or logical inputs) like as a normal oscilloscope or logic analyzer.

Therefore I use the the single time graph tool for the variables/expressions during the MCU debugging. This works for one variable/data good.
But how I could display multiple values or data in the same diagram?

I am not able to add more data with others colors.

  • Hi Seb,

    Multiple variables in the same graph... I don't think this is possible. Though you can configure the dual-time graph option. Check this out:

    Regards,

    Gautam

  • Hi Gautam,

    thanks i will try it with dual time graph the next few days.
    But i think this will only a little workaround. No solution yet.

    The symbol / icon of CCS single- time graph gives the impression to simple displays data (a blue and a read line) in one graph!

    Monitoring of multiple data is sometimes very important and necessary. I look towards VDHL simulations or MatLab/Simulink calculations where there is no problem to display multiple signals/data. CCS should handle this by the GUI because I think this is no MCU debuging limitation. So this will be a nice topic for a next CCS version.

    I try it further. My next idea is it to reference on arrays or structured variables in debug mode.
  • I agree with you Seb! This is a limitation felt by many users... I don't have an idea what limitations developers have at their end.

    As a feedback I'll forward this to a concerned person.

    Goodluck & Regards,

    Gautam

  • Hi Gautam.
    I tried the dual time graph analysis. I think that not a successfully way. It was not working in the first way.

    The best solution for multiple data is at the moment.
    - Open more single time graph an plot this in two separate graphs among each other.
    - Reduce the sampling buffer to a suitable value
    - and enable continuous sampling / refresh

    But for more as 4 my Laptop display is to small.

  • The best solution for multiple data is at the moment.
    - Open more single time graph an plot this in two separate graphs among each other.
    - Reduce the sampling buffer to a suitable value
    - and enable continuous sampling / refresh


    That's what we all do, seb :)

    Goodluck & Regards,
    Gautam