This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm using CCS Version: 6.0.1.00040 free license to debug enet_io code with EK-TM4C1294XL.
I'm getting the following error.
error #10269: output file "enet_io.out" exceeds code size limit
error #10010: errors encountered during linking; "enet_io.out" not built
Is it due to code size limit for free license I won't be able to test TivaWare codes? Do I need to purchase license or I'm missing something here.
Please help.
Thanks and Regards
Hi Vikram,
Vikram Dewangan said:Is it due to code size limit for free license I won't be able to test TivaWare codes? Do I need to purchase license or I'm missing something here.
Nope. Its free to use CCS under "Free License" for the above TIVA launchpad.
Refer this link: Limitations on Free CCS licence for Tiva C Series EK-TM4C1294XL evaluation board - Arm-based microcontrollers...
Regards,
Gautam
Vikram,
If you update to the latest compiler it will introduce a code size limit for Tiva. This issue will be resolved with the upcoming CCSv6.1 release. For now I can provide you with a license file that works around the issue. I will send you a friend request. Once you accept that I can send you a private message with the file.
Regards,
John