Other Parts Discussed in Thread: AM3352
When using CCS 6.1 is there a way to set the same project properties for both the Debug and Release configurations at the same time, e.g. when adding Include paths and libraries?
E.g. when linking a library created in a different CCS project in the workspace, the library file was referenced as "${WORKSPACE_LOC}/AM3352_SOM_platform/${ConfigName}/AM3352_SOM_platform.lib", making use of the ${ConfigName} variable, so that the same library file reference can be used for both Debug and Release platforms. However, when attempted to select a configuration of "[ All Configurations ]" I get the message that "Batch Operations are not supported":
This means that the settings have to be copied for both the Debug and Release configurations.
[I note that the stock Eclipse 3.6.1 in CentOS allows "[ All Configurations ]" to be used]