I cant find this on any of the blogs so ill post here...
Under 4.1.1.00014 ccs (plat version) installed on vista 64 everything seems ok but when i goto project properties i get a blank window. i get the project type and config fields but theyre blank and the config setting window in completely blank. This happens on both arm and msp430 projects the same.
Projects build ok as long as the defaults work but i cant change anything like include directories etc..
Iv uninstalled, reinstalled , installed under program files (x86) as well as under c:\ itself, tried running with and without admin privs. nothing makes a difference...
Any ideas?