This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I use printf() to check the progress of my code.
for example a
printf("done");
at the end. Works like a charm.
But after some runs the CIO console is quite full of text and I'm looking for another method, than using the "clear console" button.
I tried the standard C command under windows
#include stdlib.h system("clr");
but I get this error
unresolved symbol _system, first referenced in ./main.obj
Unfortunately, there is no function you can execute on the target system which causes the CCS Console view to clear.
Thanks and regards,
-George
Patrick Herda said:...
But after some runs the CIO console is quite full of text and I'm looking for another method, than using the "clear console" button.
...
Just printing a bunch of newlines might work until you find a better solution, e.g.
for(int i=0; i<1000; ++i) { printf("\n\n\n\n"); }