Part Number: MSP430F5529
Tool/software: Code Composer Studio
Hello,
I am currently fairly new in the microcontroller universe and Need them for University.
I am facing a problem considering the console and the printf command.
To make it easier, I am using the "Hello World" example file when making a new project.
The console :CIO is only opening exactly one time, if I Flash the script again i do not see the output, then I have to restart the whole Code Composer Studio.
I am using Code Composer Studio 8.2.0.00007.
I have changed the Heap to 320 and turned off the Energy-Trace function.
I hope that somebody can help me soon.
If you need further details please do not hesitate to ask.
Michael