Experts: Please help me out!
I was trying to include newer libraries through switching to a newer XDCtools (from 3_23_04_60 to 3_25_06_96). There were some error messages at the end of the switching. Now, I can't even open my RTSC projects. I can't even create an empty RTSC project. The error message is:
Error: Could not initialize class org.eclipse.rtsc.xdctools.ui.registry.RtscProductRegistry
Could not initialize class org.eclipse.rtsc.xdctools.ui.registry.RtscProductRegistry
I haven't been trying to reinstall CCS v5.3, XDCtools without any success. By the way, also have CCS v6 installed on the same PC. There wasn't any issue before that. I am using Windows 7.
Thanks,
Garry