Hi all,
For last versions of CCS (actually using 6.1.0), this problem appears continuously. When plotting anything on the graph tool (single or double time) and using a background grid, the plotted curve becomes thinner and less visible. Using "Minor grid" is even more critical because the plotted curve even "desappears". Example images are attached.
As there's no way to plot two curves on the same graph to compare them, grids are really helpfull.
Is there any way to solve this?
Thanks,
Alex