This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Project files named _cproject instead of .cproject

A customer sent me a project to review... I've just installed the latest version of CCS,  6.1.3.00033 , (usually I use IAR). It doesn't recognize that there's a project, and comparing to example projects, I see that the project files are named e.g.  "_cproject" instead of ".cproject". I also notice that in the files there are some directory paths that are not in the zipped project. Is this a version issue? A mistake in copying the project? I tried just renaming the _cproject to .cproject, but Windows won't let me do that. It also did not work to take an existing project name, replace the contents with what's in the _cproject file, and move it into the directory. Do I have to create a new project, read through the _cproject file and set everything by hand, and hope that I get all the parameters correct?