This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 6.1.3.00033 Not Installing on Ubuntu 16.04

Hey everyone,

I have used the according Wiki post when attempting to install CCS onto my Linux machine, but to no avail. After extracting the .bin executable and trying to run it, it simply blinks the cursor for a few moments then just goes away. I've tried installing 32 bit libraries, but that hasn't worked either as well as updating the libraries recommended by the instructions.

Any help you can provide would be great!

  • Suggest run the .bin executable under strace to see if the strace log reports errors about unable to load shared libraries.

    From previous experience, the Liunx installer can silently exit if some of the required shared libraries can't be found.

  • Hi,

    If you've already installed the 32 bit libraries as detailed in the wiki, please take a look at the /tmp folder and see if there's a bitrock*.log file there, and post it here. Make sure you have write and execute permissions in /tmp folder. This has been fixed in the version that's being developed now.

    Danish

  • Thank you both for your replies. It seems yesterday the support page was updated to include Ubuntu 16.04, found here. After an update that the system asked me to do, I downloaded these libraries and then libgcrypt11 separately from another site (both 64 and 32 bit versions). After that the executable worked!

  • Hi,

    Thank you for the confirmation the procedure worked for you as well. I worked on this yesterday and posted the update at the wiki page.

    Regards,
    Rafael