Hi,
I am making use of the eclipsec commands to control CCSV6 from a script.
1) When I try to import two different projects into CCS using the eclipsec command, I cannot visualize them in the 'project explorer' screen of CCS even though the command executed successfully . How do I resolve this without having to close CCS.
2) Also, is there an API that can be used to close an open project in CCS ?