Hi folks,
I recently installed CCS 6.1.3 on a new (win10) machine - CCS, nor any other TI program had previously been installed, though I have since added ControlSuite also.
I note that in my user directory there are now 3 workspace directories, named as follows: .\workspace, .\workspace_v6_1 & .\workspace_v6_1_3
Are all of them really necessary? Is it safe to remove any of them (they all have at least one or two items in them such as a .metadata dir)?
As it is there are already also CCS related directories in the user directory (.\ti & .\.TI-trace), directories in %AppData%\Local (.\Texas Instruments\CCS & .\Code Composer Studio) and a directory in C:\Program Data (.\Texas Instruments).
This is on top of the uninstall .exe. and .dat for ti_msp430pack6.3.4.4 being left in the root C:\ directory and some random user being created solely for a ControlSuite directory all outside of the supposedly self contained C:\ti directory in which CCS and ControlSuite are installed.
When a user installs other TI products as well (e.g. Fusion Designer, etc) this brings the locations of TI files & directories on a users system to an bogglingly high count!
Could at least some of these folders be collated or removed?
Moreover could the CCS development team please stop adding new directories willy-nilly all over users systems and instead use the multitude already in place (Or at the very least delete most of them upon uninstall instead of leaving them behind as is currently the case), or better yet actually reduce the number required?
Many thanks, T