This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Where is the NDEBUG defined?

Who controls the definition of NDEBUG?  I have the following code snippet:

#if defined NDEBUG
    DebugTX->print("\rPROD");
#endif

No matter what I do, the code inside the #if defined #endif executes.   In Debug build configuration I tried to do the following:

1) Did not Define the NDEBUG - the code inside the #if #endif still rins.

2) Tried to undefine as in the command below:

"/home/sporty/ti/ccsv6/tools/compiler/msp430_15.12.3.LTS/bin/cl430" -vmspx --code_model=large --data_model=large --near_data=none -O2 --opt_for_speed=3 --use_hw_mpy=F5 --include_path="/home/sporty/ti/ccsv6/ccs_base/msp430/include" --include_path="/home/sporty/HydroGuardFW/hw_1_5/miwt_os/include" --include_path="/home/sporty/HydroGuardFW/driverlib_msp430f5335" --include_path="/home/sporty/HydroGuardFW/hw_1_5" --include_path="/home/sporty/ti/ccsv6/tools/compiler/msp430_15.12.3.LTS/include" -g --undefine=NDEBUG --define=__MSP430F5335__ --diag_warning=225 --display_error_number --diag_wrap=off --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --abi=eabi --printf_support=minimal --preproc_with_compile --preproc_dependency="coap_resources/fw.d" --obj_directory="coap_resources"  "../coap_resources/fw.cpp"

Is there something really special about the NDEBUG?