Other Parts Discussed in Thread: MSP430G2553
Hi,
I am trying to send 4 bit data through 433MHZ RF. My code will transmit 0x0A if switch1 is pressed and 0x0F if switch2 is pressed.
But i am getting compilation failure and error as "error #10234-D: unresolved symbols remain".
I am using CCS 6.1.1
My code is as follows
**** Build of configuration Debug for project msp_rf_tx ****
"C:\\TI\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: ../msp_rf_tx.c'
'Invoking: MSP430 Compiler'
"C:/TI/ccsv6/tools/compiler/ti-cgt-msp430_4.4.5/bin/cl430" -vmsp --abi=eabi --use_hw_mpy=none --include_path="C:/TI/ccsv6/ccs_base/msp430/include" --include_path="C:/TI/ccsv6/tools/compiler/ti-cgt-msp430_4.4.5/include" --advice:power=all -g --define=__MSP430G2553__ --diag_warning=225 --display_error_number --diag_wrap=off --printf_support=minimal --preproc_with_compile --preproc_dependency="msp_rf_tx.pp" "../msp_rf_tx.c"
"../msp_rf_tx.c", line 57: remark #1527-D: (ULP 2.1) Detected SW delay loop using empty loop. Recommend using a timer module instead
"../msp_rf_tx.c", line 63: remark #1527-D: (ULP 2.1) Detected SW delay loop using __delay_cycles. Recommend using a timer module instead
"../msp_rf_tx.c", line 96: remark #1527-D: (ULP 2.1) Detected SW delay loop using __delay_cycles. Recommend using a timer module instead
'Finished building: ../msp_rf_tx.c'
' '
'Building target: msp_rf_tx.out'
'Invoking: MSP430 Linker'
"C:/TI/ccsv6/tools/compiler/ti-cgt-msp430_4.4.5/bin/cl430" -vmsp --abi=eabi --use_hw_mpy=none --advice:power=all -g --define=__MSP430G2553__ --diag_warning=225 --diag_wrap=off --display_error_number --printf_support=minimal -z -m"msp_rf_tx.map" --heap_size=80 --stack_size=80 -i"C:/TI/ccsv6/ccs_base/msp430/include" -i"C:/TI/ccsv6/tools/compiler/ti-cgt-msp430_4.4.5/lib" -i"C:/TI/ccsv6/tools/compiler/ti-cgt-msp430_4.4.5/include" --reread_libs --warn_sections --diag_wrap=off --display_error_number --xml_link_info="msp_rf_tx_linkInfo.xml" --use_hw_mpy=none --rom_model -o "msp_rf_tx.out" "./msp_rf_tx.obj" "../lnk_msp430g2553.cmd" -l"libc.a"
<Linking>
remark #10371-D: (ULP 1.1) Detected no uses of low power mode state changing instructions
remark #10372-D: (ULP 4.1) Detected uninitialized Port 3 in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
undefined first referenced
symbol in file
--------- ----------------
ConfigPins ./msp_rf_tx.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "msp_rf_tx.out" not built
>> Compilation failure
gmake: *** [msp_rf_tx.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****