Part Number: TMS320F28379S
Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Loaded newest Control suite ( and Code Composer (7.0.0.00043). Using V210 header files. I did the example project and got a series of errors below. Note Can.h was not part of version 200 header files
"C:\TI\controlSUITE\device_support\F2837xS\v210\F2837xS_headers\include\F2837xS_can.h", line 530: error #2638: The alignment of an array element is greater than the element size
"C:\TI\controlSUITE\device_support\F2837xS\v210\F2837xS_headers\include\F2837xS_can.h", line 533: error #2638: The alignment of an array element is greater than the element size
"C:\TI\controlSUITE\device_support\F2837xS\v210\F2837xS_headers\include\F2837xS_can.h", line 535: error #2638: The alignment of an array element is greater than the element size
"C:\TI\controlSUITE\device_support\F2837xS\v210\F2837xS_headers\include\F2837xS_can.h", line 539: error #2638: The alignment of an array element is greater than the element size
"C:\TI\controlSUITE\device_support\F2837xS\v210\F2837xS_headers\include\F2837xS_can.h", line 543: error #2638: The alignment of an array element is greater than the element size
"C:\TI\controlSUITE\device_support\F2837xS\v210\F2837xS_headers\include\F2837xS_can.h", line 546: error #2638: The alignment of an array element is greater than the element size
"C:\TI\controlSUITE\device_support\F2837xS\v210\F2837xS_headers\include\F2837xS_can.h", line 549: error #2638: The alignment of an array element is greater than the element size
"C:\TI\controlSUITE\device_support\F2837xS\v210\F2837xS_headers\include\F2837xS_can.h", line 552: error #2638: The alignment of an array element is greater than the element size
"C:\TI\controlSUITE\device_support\F2837xS\v210\F2837xS_headers\include\F2837xS_can.h", line 554: error #2638: The alignment of an array element is greater than the element size
"C:\TI\controlSUITE\device_support\F2837xS\v210\F2837xS_headers\include\F2837xS_can.h", line 561: error #2638: The alignment of an array element is greater than the element size
"C:\TI\controlSUITE\device_support\F2837xS\v210\F2837xS_headers\include\F2837xS_can.h", line 568: error #2638: The alignment of an array element is greater than the element size
"C:\TI\controlSUITE\device_support\F2837xS\v210\F2837xS_headers\include\F2837xS_can.h", line 575: error #2638: The alignment of an array element is greater than the element size
I wanted to just comment this out but could not find where it is referenced. i don't use the CAN interface. Any solutions thanks,