This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I would like to load a GEL file using the Debug Sever Scripting (DSS). Therfore I am trying to use the following JavaScript exmaple:
// Import the DSS packages into our namespace to save on typing
importPackage(Packages.com.ti.debug.engine.scripting)
importPackage(Packages.com.ti.ccstudio.scripting.environment)
importPackage(Packages.java.lang)
// Create our scripting environment object - which is the main entry point into any script and
// the factory for creating other Scriptable ervers and Sessions
var script = new ScriptingEnvironment()
// Get the Debug Server and start a Debug Session
debugServer = script.getServer("DebugServer.1")
debugServer.setConfig("DSK6416myTest.ccxml")
debugSession = debugServer.openSession("Spectrum Digital DSK-EVM-eZdsp onboard USB Emulator_0/C64xx_0")
debugSession.target.connect();
// Call of my GEL file utilizing the evaluate function
debugSession.expression.evaluate("GEL_LoadGel(myGELfile.gel)")
When executing the JavaScript I get the following error:
82 |
1938 |
0 |
SEVERE |
raise |
Evaluation of expression: "GEL_LoadGel(myGELfile.gel)" failed. identifier not found: myGELfile |
I thought I could use any GEL function in DSS. How about GEL_LoadGEL("myGELfile.gel")? Or do I overlook something?
e-schan said:debugSession.expression.evaluate("GEL_LoadGel(myGELfile.gel)")
You need to wrap the GEL file being loaded in quotes also.
Try something like:
debugSession.expression.evaluate('GEL_LoadGel("myGELfile.gel")');
You may want to use a full path to the GEL file also since I think otherwise it will default to the current windows directory (which changes all the time)
Thanks
ki
Hi Ki-Soo,
thanks for your fast response (it is amazing how fast it was).
Now I have tried your suggestion and it seems that I made one step into the right direction w/ the following result:
80 | 1938 | 0 | SEVERE | onEvent | C64xx_0: GEL: Error loading file 'myGELfile.gel': unable to open GEL file 'myGELfile.gel' |
My GEL file is located in the same folder as the javascript and that's the same folder from where I call it.
Then I tried to copy my GEL file to C:\ and changed the command to:
debugSession.expression.evaluate('GEL_LoadGel("C:\\myGELfile.gel")')
with the following result:
75 | 1938 | 0 | FINER | evaluate | ENTRY sExpression: GEL_LoadGel("C:\myGELfile.gel") |
76 | 1938 | 0 | FINER | eval | Requesting evaluation of expression: "GEL_LoadGel("C:\myGELfile.gel")" |
77 | 1938 | 0 | FINER | getScriptTimeout | ENTRY |
78 | 1938 | 0 | FINER | getScriptTimeout | RETURN 5000 |
79 | 1938 | 0 | FINER | waitUntil | ENTRY flag: GEL_LoadGel("C:\myGELfile.gel") timeout: 5000 (ms) |
80 | 1938 | 0 | SEVERE | onEvent | C64xx_0: GEL: Error loading file 'C:myGELfile.gel': unable to open GEL file 'C:myGELfile.gel' |
81 | 1938 | 0 | FINER | onEvent | Evaluated expression: GEL_LoadGel("C:\myGELfile.gel") |
Any further idea?
I can't remember how many backslashes to use (I think you might need to use four because of the escape characters). I just use a forward slash since it is easier to deal with:
debugSession.expression.evaluate('GEL_LoadGel("C:/myGELfile.gel")');
Thanks a lot! It's working now.
One last question:
How can I call a function from my GEL file that has been loaded? Let's say I would need to call myTESTS() from it.
Many Thanks in advance for your great support!
Once a GEL file is loaded, any functions defined in it can be called directly using the same expression.evaluate call:
debugSession.expression.evaluate("myTESTS()");