This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP-EXP430G2: Watching variables in assembly project (identifier not found)

Part Number: MSP-EXP430G2

Tool/software: Code Composer Studio

I'm trying to watch variables in an assembly project.  When I add a variable to the expressions window, I get the error "Identifier not found."

For example, watching testVar in the following code.

            .cdecls C,LIST,"msp430.h"       ; Include device header file
            

            .def    RESET                   ; Export program entry-point to
                                            ; make it known to linker.

            .text                           ; Assemble into program memory.
            .retain                         ; Override ELF conditional linking
                                            ; and retain current section.
            .retainrefs                     ; And retain any sections that have
                                            ; references to current section.
	    .data
	    .bss testVar, 1		    ; test data
	    .text

;-------------------------------------------------------------------------------
RESET       mov.w   #__STACK_END,SP         ; Initialize stackpointer
StopWDT     mov.w   #WDTPW|WDTHOLD,&WDTCTL  ; Stop watchdog timer

	    clr		&P1OUT
SetupP1     bis.b   #01000001B, &P1DIR          ; P1.0, .6 output


;-------------------------------------------------------------------------------
; Main loop here
;-------------------------------------------------------------------------------
Main
	    mov.b	#01h, testVar
            xor.b   testVar, &P1OUT            ; Toggle P1.0
	    call	#Delay
	    jmp		Main


Delay
	    mov.w 	#01, R14

L1	    dec.w	R14
            jnz		L1             			; Delay over?

            ret
                                            

;-------------------------------------------------------------------------------
; Stack Pointer definition
;-------------------------------------------------------------------------------
            .global __STACK_END
            .sect   .stack
            
;-------------------------------------------------------------------------------
; Interrupt Vectors
;-------------------------------------------------------------------------------
            .sect   ".reset"                ; MSP430 RESET Vector
            .short  RESET