Tool/software: Code Composer Studio
Hi, I am trying to set a floating point value through my dss script.
In my C code application I have a variable defined as follows
static float myVariable = 0.0f;
With the DSS API I can set / read this variable to any integer in any of the following ways (I am using '25' as an example but any integer will work):
myDebugSession.expression.evaluate("myVariable=25")
or
var myVariableAddress = myDebugSession.symbol.getAddress("myVariable")
myDebugSession.memory.writeData(pageNum, myVariableAddress, 25, 32)
or
I can use the .memory.writeWord() function
They are all successful in writing an integer value. However I want to write the value 0.000225 (hex 0x396BEDFA)
using any of the methods above this does not work. Does anyone know how to do this?
I am using CCS version 7.1.0.000014
Thanks,
Jack