This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
Tool/software: Code Composer Studio
I am running CCS Version 7.1.0.00016 on a Windows 8.1 Dell desktop PC. My LaunchPad is a brand new MSP-EXP432P401R. When plugged in to the PC's USB port, the launchpad runs its out of the box flashing led demo application. I have tried numerous ways of connecting from the CCS to the target board but they all fail with an "error -260" type message. On a command prompt when I run the "xdsdfu -e" command, I get a reply back that says "Scanning USB buses for supported XDS110 devices... Found 0 devices.". Also, when I look at the device manager output with the LaunchPad plugged in, I don't see any virtual COM ports created.
I tried connecting to the LaunchPad from a different laptop (with USB 2.0 ports) running Ubuntu 16.04 Linux with CCS Version 7 and ended up with the same results.
I will appreciate any suggestions on what it is that I am missing. I am new at this, so please don't assume that I have not stumbled over the obvious.