This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC2650: Error connecting to the target: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed.

Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2650

Tool/software: Code Composer Studio

I am getting an error as below when I try to debug the example project of ti Rtos, I tried the instructions given in the ReadMe.txt file but the errors still remain.

Error connecting to the target:
(Error -260 @ 0x0)
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the ReadMe.txt file there
for instructions.
(Emulation package 7.0.48.0)