This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I installed CCS6.2.0.00050_win32.exe and MSP430Ware_3_60_00_10_setup in windows 7 pc.
I could be able to create and debug projects using the installed ccsv6.2. Everything was working fine.
But when i imported a MSP430F5234 project it shows an error like this.
"Product 'msp430ware' v3.60.0.10 is not currently installed and no compatible version is available. Please install this product or a compatible version."
If you go to Windows -> Preferences on the CCS menu this will open the preferences dialog.
Then go to Code Composer Studio -> Products
Do you see MSP430Ware 3.60 listed as shown in the capture below? If not click the button to add a search location (point to the location where it is installed) and then the rediscover button.
Regards,
John