Part Number: TMS320F28335
Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
hello everyone,
I am using code composer Studio 5.3 version to control the third party designed TMS320f28335. I am a beginner to Code Composer, when I started with blinking LED program it was working. Now I am trying to control the ADC. I am getting a flash error. I referred many threads here none of them helped. I think my problem is with the target configuration. I tried ADCSOC control suite examples I am getting following errors. I am posting my JTAG test results.
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\HEMALA~1\AppData\Local\.TI\693494126\
0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
The library build date was 'Sep 4 2015'.
The library build time was '21:59:23'.
The library package version is '6.0.14.5'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '4' (0x00000004).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the FTDI FT2232 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for FTDI FT2232 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
-----[The log-file for the JTAG TCLK output generated from the PLL]----------
There is no hardware for programming the JTAG TCLK frequency.
-----[Measure the source and frequency of the final JTAG TCLKR input]--------
There is no hardware for measuring the JTAG TCLK frequency.
-----[Perform the standard path-length test on the JTAG IR and DR]-----------
This path-length test uses blocks of 64 32-bit words.
The test for the JTAG IR instruction path-length succeeded.
The JTAG IR instruction path-length is 39 bits.
The test for the JTAG DR bypass path-length succeeded.
The JTAG DR bypass path-length is 2 bits.
-----[Perform the Integrity scan-test on the JTAG IR]------------------------
This test will use blocks of 64 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Test 3 Word 0: scanned out 0xFE03E0E2 and scanned in 0xFE01E0E0.
Test 3 Word 1: scanned out 0xFE03E0E2 and scanned in 0xFE01E0E0.
Test 3 Word 2: scanned out 0xFE03E0E2 and scanned in 0xFE01E0E0.
Test 3 Word 3: scanned out 0xFE03E0E2 and scanned in 0xFE01E0E0.
Test 3 Word 4: scanned out 0xFE03E0E2 and scanned in 0xFE01E0E0.
Test 3 Word 5: scanned out 0xFE03E0E2 and scanned in 0xFE01E0E0.
Test 3 Word 6: scanned out 0xFE03E0E2 and scanned in 0xFE01E0E0.
Test 3 Word 7: scanned out 0xFE03E0E2 and scanned in 0xFE01E0E0.
The details of the first 8 errors have been provided.
The utility will now report only the count of failed tests.
Scan tests: 3, skipped: 0, failed: 1
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 2
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 3
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 4
Some of the values were corrupted - 65.6 percent.
The JTAG IR Integrity scan-test has failed.
-----[Perform the Integrity scan-test on the JTAG DR]------------------------
This test will use blocks of 64 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Test 5 Word 0: scanned out 0x5533CCAA and scanned in 0x1533CCEA.
Test 5 Word 1: scanned out 0x5533CCAA and scanned in 0x1533CCEA.
Test 5 Word 2: scanned out 0x5533CCAA and scanned in 0x1533CCEA.
Test 5 Word 3: scanned out 0x5533CCAA and scanned in 0x1533CCEA.
Test 5 Word 4: scanned out 0x5533CCAA and scanned in 0x1533CCEA.
Test 5 Word 5: scanned out 0x5533CCAA and scanned in 0x1533CCEA.
Test 5 Word 6: scanned out 0x5533CCAA and scanned in 0x1533CCEA.
Test 5 Word 7: scanned out 0x5533CCAA and scanned in 0x1533CCEA.
The details of the first 8 errors have been provided.
The utility will now report only the count of failed tests.
Scan tests: 5, skipped: 0, failed: 1
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 2
Some of the values were corrupted - 32.8 percent.
The JTAG DR Integrity scan-test has failed.
[End]
And this is one of the errors i am getting
C28xx: Flash Programmer: Warning: The configured device (TMS320F28335), does not match the detected device (). Flash Programming operations could be affected. Please consider modifying your target configuration file.
I also tried bypassing using advanced target configuration too. i am sure my board is not depleted. Because every time i get flash error i go back and try led blinking it is working. i am completely lost and confused. will be great if someone helped. 28335.pdfF28335.pdf
Thanks in advance.