This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
Here is my code:
#include <stdlib.h>
#include <stdio.h>
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include "driverlib/adc.h"
int a=100;
char buffer[10];
int length;
void UARTprint(char *cmd)
{
while(UARTBusy(UART0_BASE));
while(*cmd != '\0')
{
UARTCharPut(UART0_BASE, *cmd++);
}
//UARTCharPut(UART1_BASE, '\r'); //CR
//UARTCharPut(UART1_BASE, '\n'); //LF
}
void delayms(uint32_t time)
{
SysCtlDelay(time*(SysCtlClockGet()/3/1000));
}
int main(void) {
SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTConfigSetExpClk(UART0_BASE, SysCtlClockGet(), 115200,(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));
UARTCharPut(UART0_BASE, 't');
sprintf(buffer,"%d",a);
while (1)
{
UARTCharPut(UART0_BASE, buffer );
delayms(500);
}
}
when i run this code the output of UART only letter 't' and i cannot see the number 100 . Plz help me (sr for my bad English)
You might need to increase the heap. sprintf() is greedy.
You can also adapt K&R's itoa() code:
/* itoa: convert n to characters in s */ void itoa(int n, char s[]) { . int i, sign; if ((sign = n) < 0) /* record sign */ n = -n; /* make n positive */ i = 0; do { /* generate digits in reverse order */ s[i++] = n % 10 + '0'; /* get next digit */ } while ((n /= 10) > 0); /* delete it */ if (sign < 0) s[i++] = '-'; s[i] = '\0'; reverse(s); } #include <string.h> /* reverse: reverse string s in place */ void reverse(char s[]) { int i, j; char c; for (i = 0, j = strlen(s)-1; i<j; i++, j--) { c = s[i]; s[i] = s[j]; s[j] = c; } }