This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320VC5410
Tool/software: Code Composer Studio
Hello, we have to update and re-compile our old TMS320VC5410 projects.
"TMS320C5000 DSP Platform Code Composer Studio IDE v2" is described on our CDROM package.
We need only .out generation. No need for connecting to any Emulator.
Our purpose is code generation only. Because we can download new codes to our VC5410 board without help of Emulator.
Could you please tell me the VC5410 supported version of CCS and PC Windows?
Q1: Could you please tell me VC5410 supported version of the latest CCS?
Q2: And please tell me the VC5410 Supported PC OS(XP, Win7,Win10) ?
Q3: Can the latest CCS( also supports VC5410) import above old project files by "Import legacy CCSv3.3 Projects..." option?
We are planning to buy old PC such as WinXP if the envirnment does not run on Win7/Win10 platform.
Best regards,
ay0689
Hello, Yordan-san,
thank you for your prompt reply and arrangement.
I am waiting for C5000 team's reply.
Thanks and best regards,
ay0689
Hello,
ay0689_2 said:Q1: Could you please tell me VC5410 supported version of the latest CCS?
See: https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/604690/2225305
ay0689_2 said:Q2: And please tell me the VC5410 Supported PC OS(XP, Win7,Win10) ?
See: http://processors.wiki.ti.com/index.php/System_Requirements
ay0689_2 said:Q3: Can the latest CCS( also supports VC5410) import above old project files by "Import legacy CCSv3.3 Projects..." option?
The latest CCS that you can use for C54x is CCSv5.5. You should be able to import CCSv3.3 projects in there. It gets a little more tricky if you project is a DSP/BIOS project but overall it is supported.
Thanks
ki
Hello Lee-san,
thank you for your clear reply.
CCSv5.5 is the last version to support C54x.
processors.wiki.ti.com/.../Download_CCS
Below are the system requirements for Code Composer Studio v5
Minimum | Recommended | |
Memory | 1GB | 4GB |
Disk space | 300MB* | 2GB |
Processor | 1.5GHz single core | Dual core |
As the first step, we will check our CCS2.1 Based project files by CCS5.5/Windows7 PC.
If the import to CCS5.5 is failed or many modifications are needed, we may purchase Windows XP PC to build CCS2.1 Environment.
However, we have one unclear point.
Is CCS V2.1 worked on WindowsXP?
Thanks and best regards,
ay0689