This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi,
From the loadRaw Doc:
public void loadRaw(int nPage, long nAddress, java.lang.String sFilename, int nTypeSize, boolean bByteSwap)
throws ScriptingException
nAddress
- is the first address in the block.nPage
- the memory page. Use one of Memory.Page enumeration.sFilename
- specifies the name of the file that will store the target data.nTypeSize
- specifies the type size of the data. Affects how data is byte-swapped to account for differences in host and target endianess. For example: if the target is big endian (the host is always little endian) and you specify nTypeSize = 16 then the upper and lower bytes are swapped after loading the file - but before writing to target memory.bByteSwap
- Force a byte-swap of the data before writing to target memory. If Host and Target are difference endianess - this will effectively disable the automatic endianess conversion.ScriptingException
Can You please explain the meaning and usage of the nTypeSize - i could not figure out how it works and what values should accept (when i loaded a file and set it to 8 assuming it means loading the file byte by byte it seemed to write to memory that exceeds the file length while if ste it to 32 it seemed ok - why ?).
Also how this relates to the bByteSwap
parameters and how this also is being used.
Thanks
Guy
Hi,
I am currently using TDA3xx / TDA2xx
I have already looked at the main document and since the documentation there is very general and missing a lot (i.e. description of what exactly each of the functions parameters do) i posted the question.
I hoped you would have a more detailed document and/or can help from your own knowledge
Thanks