This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CCS 7.2 Installer widget error

Tool/software: Code Composer Studio

Hello.
I have problem with installer. I cannot install CCS 7.2 because of "unknown widget" when editing proxy field.

I'm using Windows 7 x64 Enterprise SP1
Installer version: ccs_setup_7.2.0.00013

Error message:

unknown widget ".wizard.steps.fInstallDirPane.clientarea.proxyframe.port"
unknown widget ".wizard.steps.fInstallDirPane.clientarea.proxyframe.port"
    while executing
"Widget::cget $path $option"
    (procedure "Entry::cget" line 5)
    invoked from within
"Entry::cget .wizard.steps.fInstallDirPane.clientarea.proxyframe.port -state"
    ("eval" body line 1)
    invoked from within
"eval [linsert $larg 0 Entry::$cmd $path]"
    (procedure "Entry::_path_command" line 3)
    invoked from within
"Entry::_path_command .wizard.steps.fInstallDirPane.clientarea.proxyframe.port $cmd $args"
    (procedure ".wizard.steps.fInstallDirPane.clientarea.proxyframe.port" line 1)
    invoked from within
"$w cget -state"
    (procedure "tk::EntryButton1" line 9)
    invoked from within
"tk::EntryButton1 .wizard.steps.fInstallDirPane.clientarea.proxyframe.port 286"
    (command bound to event)
  • Are you using the web installer? If so, could you please try the offline installer and let us know if that is successful?
    You can download the offline installer from here.

  • SOLUTION:

    Uninstall all installations of CCS and remove its base directory with all data. Then install CCS using offline installer.
    Installing over previous versions may cause problems and probably will fail.