This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC2650: Problem running a project in CSS cloud - project does not have a target - but it is a demo project from projectzero

Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2650, CC2640, CC2540

Tool/software: Code Composer Studio

Session 1508945208400_00013935

I'm trying to install the ProjectZero application onto my CC2650 Launchpad as per the Academy video https://training.ti.com/simplelink-academy-develop-your-bluetooth-low-energy-project (about 8.30mins into the video)

I've had to muddle through a little because the Resource Manager does not seem to list files in the same way as in the video, but all was going well until I needed to program the device in the Launchpad with the ProjectZero software from CSS cloud.

It builds okay, but I get the error "Run Failed. The project does not have a target type"

I'm new to CSS so a bit stuck - googling this error did not seem to help.

Note: The academy video is for CC2650 which I have, but the only projectzero project I could find was for the CC2640 (apparently they are cross compatible so assumed this would be okay)

Please help.
thanks
Sian