Using: ccsv4 4.1.2.27, (and tried 4.1.3.38) with win 7-64.
When trying to see build steps (Project -> Properties -> C/C++ Build -> Build Steps -> Post-build Steps:
1) can't see the "Post-build Step" area unless I resize window, but then it doesn't have the choice to make Intel hex file anymore (used to).
saw this in a forum some place and can not find it again (what forum was that in?)
2) Is problem with Win-7 win7-64 or what? Used to work until I updated CCSv4 to last version or 2 ago.
Is there anything I can do? ie. manullay edit a file to add it in?
3) I tried turningoff User Access Control -> no help.
running in XP comp. mode, but win says eclipse is not compatable.
Anyone else see this?
thanks,
dan