Part Number: MSP-EXP432E401Y
Tool/software: Code Composer Studio
With CCS 8.0.0.00016 and TI Emulators 7.0.188.0 running under Windows 10 was attempting to use Statistical Function Profiling to investigate when a program running on a MSP-EXP432E401Y crashes, using the on-board XDS110. In the Statistical Function Profiling was selecting the Sampling Interval, and setting a manual Clock Frequency of 120000000 for the Receiver Settings.
To try and get more information about the symptoms of the program crash was attempting to lower the Sampling Interval for the Statistical Function Profiling (the default is 1024 cycles). Using 896 cycles can capture information. However, if attempt to use 832 cycles (or lower) then when pause the program then CCS becomes non-responsive and have to kill CCS.
The same problem with CCS hanging:
a) Happens on a different Windows 10 PC running CCS 7.2.00013 with TI Emulators 7.0.188.0.
b) Can be repeated using the unmodified tcpecho_MSP_EXP432E401Y_tirtos_ccs example from simplelink_msp432p4_sdk_2_10_00_14.