This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: Code Composer Studio 6.1.3



Tool/software: Code Composer Studio

hello ,  when i am trying to import project legacy to CCS ,  i receive this error : 

See details below.
Error: A project with the name 'pwmm' already exists in the workspace!

my Code Composer Studio 6.1.3

please any advice 

  • Hello,
    The error means that a project of that name already exists inside the workspace FOLDER. So even of it does not appear in the Project Explorer view, please check to see if there is a physical folder of the same name inside the current workspace folder

    Thanks
    ki
  • Hi,

    As Ki mentioned there should be a physical folder inside the workspace folder with that name. You know that every new project in CCS is correspondingly a new physical folder inside the workspace folder. So related to the error you faced with, the solution is to find the folder with that similar name and try to rename it or instead of it, try to choose another name for the new project you want to create.


    Regards,
    Hossein