Part Number: TMS320F28379D
Tool/software: Code Composer Studio
Hello,
I am having a difficult problem. I had used the adc_epwm project to create a custom project that allowed for both RAM and Flash-based debugging. Everything seemed to be working just fine last week; however, a co-worker of mine reported that he was having trouble running the code.
When I connected to the development board to try to help, I found that I could not JTAG. The error I am getting states:
Error connecting to the target:
(Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 7.0.188.0)
And, there is just a solid green light on the development board (D4). It's as if the development board is "bricked". What am I doing or did I do wrong?
Thank you,
Noah