Part Number: PGA970EVM
Other Parts Discussed in Thread: USB2ANY, PGA970, PGA900
Tool/software: Code Composer Studio
Hi my name is Hector A Ochoa, and we need some help using a temperature sensor on the PGA970EVM. We just acquired the PGA970EVM board with the USB2ANY adapter for a research project. We are trying to take measurements of displacement using an LVDT, and Temperature using a voltage divider circuit with one of the resistors been a thermistor. We have tested the LVDT with the GUI interface, and we are able to get some measurements. The problem is that it seems that using the GUI interface, we won’t be able to measure both parameters and store the information. We are thinking of using CCS to take the readings directly from the registers and store them into an SD-card. However, we haven’t been able to load any code into the PGA970EVM board. Is there a special procedure to load the code? Or do we need something else besides the USB2ANY adapter? If you can point us in the right direction, I will really appreciate it.
Best Regards,
Hector A Ochoa