Part Number: CODECOMPOSER
Tool/software: Code Composer Studio
I cannot install Code Composer Studio 8.2.0.00007 (or any previous version back to v6, online installer or offline installer). When I run the installer I get a pop-up message that says:
"Installer Initialization Failed."
"The installer will now exit."
There is a little bit of history here. I tried to install it yesterday (online and offline installers) and it would give the above message. Inexplicably one time the online installer started installing, and I couldn't tell what I had done differently. The installer ran for several hours but didn't get past maybe 20%, and I let it go overnight.
By this morning it had made no progress so I cancelled the install. However it didn't seem to uninstall correctly because it was still listed in the the Windows Add/Remove Programs list. When I clicked Uninstall it said that "ccs_uninstall.exe" could not be found. I tried to install again none of the installers would get past the error screen. I went into regedit and removed the corresponding registry key for the Uninstall program list, and this of course didn't solve the problem.
Here are a few more details. The installation seems to stop before writing any logs (as far as I can tell). The MD5 hash matches for the offline installer. I am running Windows 10 Enterprise Version 10.0.16299 Build 16299.
Any thoughts? I am stuck.