Part Number: LAUNCHXL-CC2640R2
Tool/software: Code Composer Studio
Hi forum,
about runtime object view I have two questions:
1) In ROV my stackPeak is sometimes higher than the displayed value and return fast to a lower value that dont change for a long time (1-5min). I thought the stackPeak represents the maximum stack in use since runtime, that was my assumption, but it is wrong. Is there a possibility to get this value, also the highest value? Or do you make try and error too and get the optimum stack size empirical?
2) In my application there are 4 task. Once in 5..10min there happened rov->task->detaied->blockedOn a red flag "blockedOn Internal Error" message. What does it mean?
Hint to 2): at the other time it show the normal "blockedOn Semaphore: 0x20002288" in white / or yellow (changestate). And the application has normal function, works well, dont hangup.
best regards,