Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Hello.
I have a problem while I follow TIDM-BIDIR-400-12 design.
I can run the debug mode with internal xds100v1.
I have JTAG emulator which is based on xds200.
I want to use JTAG emulator for the TIDM-BIDIR-400-12 design.
In this boot mode selection table above, I can run with the onboard xds100v1 in mode 1,SCI mode.
I think If i want to run with JTAG emulator, then I should activate TRST as '1'.
In tidrhs9 document, I can find the TRST related jumper called J13.
I dis-populated that J13 jumper, tried to run Test connection button in tmsf28035.ccxml file.
But error message showed that...
[Start: Texas Instruments XDS2xx USB Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\user\AppData\Local\TEXASI~1\CCS\
ti\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
The library build date was 'Jul 27 2016'.
The library build time was '17:54:51'.
The library package version is '6.0.407.3'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '13' (0x0000000d).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
This emulator does not create a reset log-file.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-230' (0xffffff1a).
The title is 'SC_ERR_PATH_MEASURE'.
The explanation is:
The measured lengths of the JTAG IR and DR scan-paths are invalid.
This indicates that an error exists in the link-delay or scan-path.
[End: Texas Instruments XDS2xx USB Debug Probe_0]
what can I do for this error? Am I configure the correct jumper?