This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS / TMS320C5545:C5545 BoosterPack Software document

Part Number: TMS320C5545


Tool/software: Code Composer Studio

Hi,

This is my first use of this programming software, there are many things that I don't understand.

Now I am following the C5545BoosterPackSodtware document, in the 2.3.2 Build Procedure part.

In the step4,

4. Navigate to the C55xx CSL source folder (Default path - C:\ti\c55_lp) and import the following projects: (a) C55XXCSL_LP (b) atafs_bios_drv_lib 

Is it use the same way as the step1-3? Using the Project → Import CCS Projects?

In the step5,

5. Navigate to C:\ti\c55_lp \ c55_csl_x.xx\inc\csl_general.h and change the following macro definitions:
#define CHIP_C5517 to //#define CHIP_C5517

#define CHIP_C5505_C5515 to //#define CHIP_C5505_C5515

#define CHIP_C5535 to //#define CHIP_C5535


And when I following step5, I find the second and third one. But there seem no #define CHIP_C5517 in the original document, which one should I change?

In the step6,

6. Build C55XXCSL_LP and atafs_bios_drv_lib in both Debug and Release modes.

How to build them in Debug and Release modes?

--------

Now I am in step5, how can I do to solve these problems.

Thank you!
  • Hi Yutong,

    You should follow the same steps for C55XXCSL_LP and atafs_bios_drv_lib as it is described in sprui92.pdf.
    If you search for "#define CHIP_C5517" in csl_general.h you will find it. You should comment all macros CHIP_C55xx except "#define CHIP_C5545".
    You are free to use each one of both models but "Debug" is recommended for developing and debugging your source code.
    Also the linked below threads should be useful about C55XXCSL_LP issues:
    e2e.ti.com/.../510293
    e2e.ti.com/.../444572
    e2e.ti.com/.../443289

    Regards,
    Tsvetolin Shulev
  • Thanks for your help! It solves my problems.

    And now I am in,

    2.3.2.1 Building Diagnostic Test Binary

    1. Right click on the project ‘boostc5545_diag_test’ and set ‘Build Configurations’ to ‘SD_BOOT’.

    2. Right click on the project ‘boostc5545_diag_test’ and select the Build Project option.

    3. bootimg.bin will be created under c55xx_diagnostics/bin folder.

    When I run the second step there are many error shows in Description.

    I see in the step3, it says that there will be a bootimg.bin in the document.

    In my document, there has one, but I see the time is 2016/9/13. So I think maybe there are some problems?