This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi all,
I installed the the new simple link package simplelink_cc13x2_26x2_sdk_2_40_00_81 and simplelink_cc13x0_sdk_2_40_00_20 at a installed version of th Code Composer 8.3.0. Noe the resource explorer tried to implement the new packages and the it stops working
1. Try to implement it:
The the resourse explorer stop with error.
I unistalled everything and reinstalled everything. Nothing helped.
Please help.
BR Noge
Hi ki,
yes I´ve readed it again, deleated the caches, uninstall the latest Simple link packages. Everthing works fine. I've installed the CC13x0 simple link 1.60, 2.10, 2.20, 2.30, 2.40, CC26x2 Simple link 2.30. Everythin ok. Now I installed the simplelink_cc13x2_26x2_sdk_2_40_00_81. The resource explorer crashes again.
BR Noge