This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1352R: Resource Exploren don't work after installing simple link package

Part Number: CC1352R
Other Parts Discussed in Thread: SIMPLELINK-CC13X2-26X2-SDK

Tool/software: Code Composer Studio

Hi all,

I installed the the new simple link package simplelink_cc13x2_26x2_sdk_2_40_00_81 and simplelink_cc13x0_sdk_2_40_00_20 at a installed version of th Code Composer 8.3.0. Noe the resource explorer tried to implement the new packages and the it stops working

1. Try to implement it:

The the resourse explorer stop with error.

I unistalled everything and reinstalled everything. Nothing helped.

Please help.

BR Noge