Other Parts Discussed in Thread: TMS570LC4357
Tool/software: Code Composer Studio
Hello Expert,
I am trying to collect the ETM trace data from TMS570LC43x using XDS560V2 Pro Trace, but no data is collected. Could you please check is I missed any anything in my configuration.
Device used: TMS570LC4357
PCB: HDK with 60-pin MIPI connector
Trace tool: XD560V2 Pro Trace
CCS: 8.x
1. The device is connected with XDS560V2 Pro emulator.
2. The HW Trace Analysis is configured as below:
3. Start the trace collection in trace viewer:
4. Load the rtiBlinky example code to the flash, and execute the code from flash, the LED on the HDK is blinking.
5. Stop trace collection, but there is no data collected
As showed in the screenshot, no data is collected. I don’t use PLL, so the CPU speed is 16MHz only. Do I need to configure or initialize the ETM and TPIU in my MCU to use the trace feature of XDS560V2 Pro Trace?
Thanks for help