I am running windows 7 64 bit and I am missing screens in the macros tab (see printscreen). I have installed CCS4 two more times in different locations and done all the updates and I still have the same problem of missing the macros screens. Also, when I first started using CCS4 ver 4.1, all the screens were missing in the C/C++ build (see also the link to the post below. Over the summer TI sent me two JRE files to fix the problem and those two JRE files are still required after installing CCS4.1 from the DVD and doing all the online update to 4.2. I don’t know if the JRE patch to fix the C/C++ build screen from the original fix is compatible with 4.2 but that’s just a guess.
Doug

Original problem fixed by the JRE files.
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/54429/195359.aspx#195359