This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2640: Load SimpleBLEPeripheral into a ccsv9 Project

Part Number: CC2640


Tool/software: Code Composer Studio

How do I load SimpleBLEPeripheral into a ccsv9 project?

Before my PC crashed, I followed this procedure to load SimpleBLEPeripheral into my project:

In ccsv7, download and install (with default settings) TI BLE SDK v2.x
Click View > Resource Explorer Classic (aka TI Resource Explorer) and do the following:
 Enter search keyword: simple
 Find and expand SimpleBLEPeripheral
 Copy SimpleBLEPeripheralStack into project
 Copy SimpleBLEPeripheralApp into project

To restore my PC, I upgraded to 64 bit Windows 10 and installed ccsv9, but I can't follow my ccsv7 procedure.

First question: How do I access Resource Explorer Classic or equivalent in ccsv9?

Second question: How do I load SimpleBLEPeripheral into my project in ccsv9?

I am programming a CC2640F128, not R2.

  • ad 1) use current Resource Explorer

    ad 2) use Project -> Import CCS Projects...
    and go to the path where your TI BLE SDK v2.x is installed
  • The older BLE SDK is not supported with the newer Resource Explorer. And Resource Explorer Classic is no longer included with CCS v9.

    So you have a couple of options:

    1) Use CCS v8 with Resource Explorer Classic 

    2) Use CCSv9 and import the project as suggested by Tom. Go to CCS menu Project->Import CCS Projects, browse to the example directory inside the BLE SDK (eg: C:\ti\simplelink\ble_sdk_2_02_02_25\examples\cc2650lp\simple_peripheral) and select the projects to import

  • I have to select the FOLDER of the project. I sometimes take instructions a bit too literally.

    Thank you both for your advice!